Hi,
I want to make OV5640 Camera Operate with TI-RTOS using VIP subsytem.
Inspecting the TI-RTOS SDK, I found that there is an example for each of:
1- Capturing from Camera using VIP (pdk_am57xx_1_0_16/packages/ti/drv/vps/examples/vip/captureVip)
2- Capturing from Camera using VIP and Displaying it (pdk_am57xx_1_0_16/packages/ti/drv/vps/examples/loopback)
But none of these examples work with OV5640.
Inspecting the loopback example, I found that the most similar Camera to OV5640 is OV2659 which is already supported in TI_RTOS SDK.
Question: Is that similarity correct? (I could not find OV2659 datasheet, I would be thankful to give me its link if it's publicly available)
Inspecting Loopback example, I guess that to add support for OV5640 so that I can show its captured data on dispaly using Loopback example, I must add an OV5640 driver in (pdk_am57xx_1_0_16/packages/ti/drv/vps/src/devices) which must be compatible with FVID2 and finally add an entry for it in Loopback example.
Question: Is my guess right Or I need to do more things?
Question: are there any OV5640 camera driver developed for TI-RTOS?
Thanks in advance