hi
I'm using a custom platform based on j6entry evm.
Using 8-bit NAND (MT29F1G08ABAEAH4-AITG) with Page size 2048 and Spare size 64, nand boot is successfull.
But, using Using 8-bit NAND (MT29F2G08ABAGAH4) with Page size 2048 and Spare size 128 bytes, nand boot is fail.No output from uart。
MT29F2G08ABAGAH4 datasheet see attachment.
Is the Dra71x supported the nand with 2048 bytes + 128 spare ?
If supported, please tell me the specific configuration method?