Hi TI Team:
This is regarding the layout guidelines for DDR3 interface for TMS320C6678 multicore DSP processor.
In section "6.3.1.4 - Routing Rules – Address and Command Lines (SDRAMs)" of the the appnote "DDR3 Design Requirements for KeyStone Devices (sprabi1c)", it tells us to route single ended address and command lines with 50 ohms track impedance.
However, in section "6.2.1 External Terminations – When Using Read and Write Leveling", it clearly tells that VTT fly-by terminating resistors of the value 39ohms to 42ohms should be used.
These two recommendations are confusing because a fly-by active termination resistor value and the corresponding trace impedance value should be equal.
As per my understanding, the statement regarding trace impedance of 50ohms is wrong since DDR3 signals are typically routed with 40 ohms trace impedance.
Kindly clarify.
Thanks,
Binayak.