The AM5749 can run at four speeds: 750 MHz, 1000 MHz, 1176 MHz, and 1500 MHz. All my years of experience are with writing my own bare-metal code for the bootloader (and processor initialization code) and then running under SYS/BIOS, so when booting the AM57x via U-Boot/Linux from the SDK, at the user level (well, root user), how do I both check the current CPU speed and set the current CPU speed?
In your kernel, cpufreq does not exist under /sys/devices/system/cpu/cpu0 (nor for ./cpu1 for that matter) which is what I was told to check by someone else.
It's imperative that I am running at 1500 MHz when active (due to the real-time nature of my app), and it's preferable to down-clock to 750 MHz when I'm idle to reduce the chip's power consumption to reduce the heat.