This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

AM5729: Still reachable memory leak with OpenCL examples on BeagleBone AI

Prodigy 80 points

Replies: 4

Views: 105

Part Number: AM5729

Hi all,

Like the title says, I have a BeagleBone AI running the latest (as of writing) [Debian Buster image](https://beagleboard.org/latest-images). It seems there is a memory handling issue when I try to run the openCL examples found under `/usr/share/ti/examples/opencl`. See the attached valgrind output.

Is this a known issue, or is this something I need to take up with the BeagleBone folks?

Thanks,

Matt

opencl_fftexample_valgrind.txt

  • Hi,

    Debian is not supported by TI. Please contact the Debian community on www.beagleboard.org 

     

    Best Regards
    Biser
  • In reply to Biser Gatchev-XID:

    Hi Biser,

    My apologies - thanks for the suggestion.

    I've been advised to try using the TI Processor SDK image (v06.02) on an SD card, but I'm still getting memory leaks running the same example. See attached.

    Thanks,

    Matt

    EDIT: I should mention that I have not been successful in using v06.03 on an SD card.

    opencl_fftexample_valgrind_tipsdk.txt

  • In reply to Matt Anderson:

    I was finally able to load the v6.03 SDK onto an SD card and try again, and I get the same memory leak as in v6.02. Attached.

    opencl_fftexample_valgrind_tipsdk_0603.txt

  • In reply to Matt Anderson:

    Matt,

    We took a look into your valgrind report:

    ==1299== possibly lost: 961,415 bytes in 1 blocks
    This is from libelf. We did call elf_end() and it did return 0, which means the resources should have been released by libelf. Valgrind did report "possibily." Even if it is not released, the corresponding function is called only once and the memory is one-time allocation per process.

    ==1299== still reachable: 796 bytes in 11 blocks
    These are from various underlying libraries that OpenCL host runtime depends on. For example, inter-processor communication library. These memories are only allocated once per process and they will be deallocated when process terminates. In other words, it doesn’t matter if you run your kernel 100 times or 100 million times, these memory allocations will not change.

    The summary is there should be no concerns here. A "concerning" memory leak would be that the runtime is allocating more and more new memory for the same use, while not releasing old memory as program runs longer and longer. This is not the case for the warnings that are flagged.

    Best regards,

    Dave

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.