Hi,
We developed and produced board based on IDDK5749 design, but added SATA and 2GB RAM without ECC. All hardware work very fine. But we need launch (we ready to recompile for this platform) our technological x11 based software. As i know X11 support not provided for current PSDK, but recipes contain all x11 stuff.
I`m tried to make image based on processor sdk v4 x11 branch.
Follow all instructions, similar to build for PSDK5 and PSDK6 (succesfully compiled on my ubuntu 16.04)
The only X11 supported Processor SDK version is processor-sdk-04.01.00.06-x11-config.txt.
You can build it on your host machine in this way.
$ sudo apt-get install git build-essential python diffstat texinfo gawk chrpath dos2unix wget unzip socat doxygen libc6:i386 libncurses5:i386 libstdc++6:i386 libz1:i386
$ sudo dpkg-reconfigure dash
Select "No" when prompted.
$ wget releases.linaro.org/.../gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf.tar.xz
$ tar -Jxvf gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf.tar.xz -C $HOME
$ git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk
$ cd tisdk
$ ./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-04.01.00.06-x11-config.txt
then i`m download sources snaphot:
$mkdir downloads
$ cd downloads
$ # Assuming src file downloaded to $HOME/Downloads
$ tar xvf $HOME/Downloads/<target-board>-linux-sdk-arago-src-##.##.##.##.tar.xz
$ <target-board>-linux-sdk-arago-src-##.##.##.##/get_build_sources.sh <target-board>-linux-sdk-arago-src-##.##.##.##/source_pkg_list.txt
then i try to build:
cd ../
$ cd build
$ . conf/setenv
$ export PATH=$HOME/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:$PATH
MACHINE=am57xx-evm ARAGO_RT_ENABLE=1 bitbake arago-base-tisdk-image
there are error with external-linaro-toolchain:
ls: cannot access '/home/rock/tisdk4/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago36/image/lib/libanl.so.*': No such file or directory
WARNING: /home/rock/tisdk4/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago36/temp/run.do_install.28188:1 exit 2 from 'l=$(ls $f.*)'
ERROR: Function failed: do_install (log file is located at /home/rock/tisdk4/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago36/temp/log.do_install.28188)
I`m checked that in image folder exist libanl-2.23.so.
Main question: how i can receive working image for my board without wayland, but with x11 server.
I`m try to compile xwayland on PSDK603, but receive to many errors.
Please provide some instructions.