Goal: Use timer 3 to generate a free running counter at 1 Mhz.
Input clock frequency: 187.5 MHz (SYSCLK2)
Timer Mode: dual 32-bit chained mode
Question: What is the prescale period value that will result in TIM12 count at 1 MHz?
Problem: Prescaler needs to be 187.5 but it needs to be a whole number.
Is there an alternative method to accomplish the same goal?