Tool/software: Code Composer Studio
Hi,
The customer wants to create SD Card boot image. Can they get the Windows script to create SD Card boot image ".img" file ?
They referred to “1.1.11. Windows SD Card Creation Guide” in the Processor SDK RTOS Software Developer’s Guide.
They found Linux script “create_img.sh” and “create-sdcard.sh” in the directly of
C:\ti\processor_sdk_rtos_am335x_5_01_00_11\processor_sdk_rtos_am335x_5_01_00_11\bin, but they need Windows script, but couldn’t find Window script.
Do you have a Windows script to create SD Card boot image ?
They should use create_img.sh ?
If so, is it OK to use .out file built by CCS as an input file for create_img.sh ? Should they add any option during building files on CCS ?
Could you tell them some example of command line use case of create_img.sh ?
Thanks and regards,
Hideaki