Hi Sitara support Team,
According to Figure 15-70, GPMC_CLK stops when CYCLE time completes.
My customer would like to confirm this as it affects the design of the receiver side FPGA.
Is it possible to set GPMC_CLK not to stop?
Best regards,
Kanae
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sitara support Team,
According to Figure 15-70, GPMC_CLK stops when CYCLE time completes.
My customer would like to confirm this as it affects the design of the receiver side FPGA.
Is it possible to set GPMC_CLK not to stop?
Best regards,
Kanae
Hi Sitara Support Team,
I refer the this thread, but it did not solve the last question.
*****
is it not possible to use gpio6_16.clkout as GPMC_CLK in the following cases?
GPMC_FCLK = 266 MHz
GPMCFCLKDIVIDER = 0x2: GPMC_CLK frequency = GPMC_FCLK frequency / 3
GPMC_CLK = 88 MHz
******
I would like to know the answer, if it is not possible to set GPMC_CLK to keep running.
Best Regards,
Kanae
Kanae,
GPMC_CLK cannot be free running. Customer can use GPIO6_6.CLKOUT1 as an "always-on" alternative, but note this clk cannot be used to replace GPMC_CLK to latch data from the bus.
More details can be found in this post here: https://e2e.ti.com/support/processors/f/791/p/674641/2490132?tisearch=e2e-sitesearch&keymatch=gpio6_16%2520programmed#2490132
Have a great day!
Best Regards,
Shiou Mei
Hi Shiou Mei,
Thank you for your reply.
I refer the post you informed.
Best regards,
Kanae