Other Parts Discussed in Thread: UNIFLASH
Hi Team,
As you know, Uni-flash is used to program the emmc flash on board. Here we want to use off-board emmc flash write way, which means use a in-dependent programmer to write the image, take Linux processor SDK prebuilt-image as example,
Are the images which will be programmed to emmc flash same as prebuilt-images which can be used to SD card create? or need to do some convert? Do you have some guide how to program the image to emmc flash? disk partition, offset configuration etc or it is similar as SD card create patch as emmc and SD have similar interface and protocol.
For NAND flash, seems we can read the written NAND flash image from the flash, and then write-back it to NAND-flash, can we use the same way to read the written image in emmc flash and then write-back to emmc flash through the programmer?
Thanks
Thomas