• Resolved

TDA4VM: Regarding boot up of custom board with new SDK 07 and patch

Expert 1110 points

Replies: 35

Views: 387

Part Number: TDA4VM

Dear TI,

I have following error during the boot with custom board using SDK 07, please see the attachment. Can you please help me to figure out which DT has the issue ?

Also, I found a small error related to make u-boot which is in the rules .make , in "arm-none-linux-gnueabihf" you have missing none word which fails the make.

# Add CROSS_COMPILE and UBOOT_MACHINE for the R5
export CROSS_COMPILE_ARMV7=$(LINUX_DEVKIT_PATH)/sysroots/x86_64-arago-linux/usr/bin/arm-none-linux-gnueabihf-
UBOOT_MACHINE_R5=j721e_evm_r5_config



Regards

Manish