Hi Siatara support Team,
This post is related the following thread.
e2e.ti.com/.../3388052
My customer evaluates their custom board using AM3357
and the software is based on PROCESSOR-SDK-RTOS-AM335X 04_02_00_09.
They would like to make clear the following register values.
Q1:
Control module: gmii_sel has a default value of 0 when not in use,
but the code for pdk when using the port sets rgmiiX_idmode to 0 (Reserved),
which is not the default value, is this correct?
Q2:
Similarly, are the following settings for rmiiX_io_clk_en correct?
-If not used or not used by RMII or RGMII, it is set 1 same as the default value.
-When using MII or GMII, it is set to 0.
Please answer as this case is used SR2.0 or higher.
Best regards,
Kanae