Dear experts,
I am helping customer to develop TIDL applications. In one use case, their model will output more than 15 output_tensors. When we integrated with OpenVX( using tivxTIDLNode), we find that there is a limitation in max number of parameters. Could you please suggest which micro to change to enable more parameters?
Here is the log:
APP: Init ... Done !!!
0.000923 s: VX_ZONE_INIT:Enabled
0.001404 s: VX_ZONE_ERROR:Enabled
0.001680 s: VX_ZONE_WARNING:Enabled
0.002611 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!!
0.006030 s: VX_ZONE_INIT:[tivxHostInit:44] Initialization Done for HOST !!!
0.684712 s: VX_ZONE_ERROR:[tivxAddKernelTIDL:260] invalid values for num_input_tensors or num_output_tensors
0.685161 s: VX_ZONE_ERROR:[tivxTIDLNode:101] Exceeded max parameters for a kernel
I found a micro: "TIVX_KERNEL_MAX_PARAMS" == 16 in tiovx/include/TI/tivx_config.h.
Please help to confirm if it the correct place. Thanks!
Thanks & Best Regards!
ZM