Hi,
I'm using TDA2x Custom board with VisionSDK 3.07.
I want using GPIO in Linux usecase.
The GPIO I want to use is GPIO7_27.
so UART2_TXD_MUXMODE set to 0xE in CTRL_CORE_PAD_UART2_TXD.
Q1. Is the register setting impossible on Linux? Segmentation fault occurs on Linux. So, I did it at IPU side.
Q2. Is there an example of GPIO provided by TI?
I found some gpio examples. but it runs on RTOS. so i want linux example.
Best regards,
Lee.