Other Parts Discussed in Thread: AM5718
Hello Guys,
This is Milav Soni From Teq Diligent.
I have a Embedded Board which have "AM5716AABCDA" Processor.
In hardware we select Booting option like :-
1st --> SD
2nd --> eMMc
PMIC is also working fine and gives output as per power sequence defind in uP Datasheet.
We have also see 20Mhz Clock signal in Oscilloscope.
We have also see reset signal and it is in good voltage level.
But when i make sd card from "am57xx-evm-linux-rt-06.03.00.106.img" and See the log over UART3 console,
I didnot see any thing over there.
so i want to know that what is data value for ROM Code, means how i can verify that my processor is booting very well or not?
is there any UART console for init ROM code for the same image and uP.?
so please help me to sort out this question.
+)(, +*,- -