Hi,
My customer is using C6657 in legacy product and needs to do some DDR3 debug.
As the software is a bit old one (MCSDK v2.1.2.6), no one at customer knows implementation in details.
Customer wants to know exact source codes where below DDR3 memory controller registers are configured.
Base address: 0x2100:0000 DDR3 EMIF configuration
Offset: 000h to 120h DDR3 Memory Controller Registers
Could you point me the source file and line# in MCSDK?
Thanks and regards,
Koichiro Tashiro