Hello everyone,
i recently installed tisdk4.02 in my laptop and tried to run setup file . but it is not happening smoothly as earlier it asking me for proper dependencies to be installed . so i tried to install them but i found recently ntfs-kernel-server packages which version will get fetched while running setup file is showing that unable to fetch. i checked them in ubuntu archive and it seems to be that package is removed from archive so now
1. can i go for other ntfs-kernel-server versions to run setup file ? if so any one tell me how?
2.in my old system i have those packages already installed can i copy those packages from that system to laptop if so how to do that?
3.and once if all the things if become is that enough for higher versions of sdk also or for higher versions we have to install another dependencies?
please some one help in this matter.
and here is how errors are message coming to me...some one suggest me proper solution or alternate for this.
Do you want to continue? [Y/n] y
Err:1 in.archive.ubuntu.com/ubuntu xenial-updates/main amd64 nfs-common amd64 1:1.2.8-9ubuntu12.2
404 Not Found [IP: 43.255.166.254 80]
Err:2 in.archive.ubuntu.com/ubuntu xenial-updates/main amd64 nfs-kernel-server amd64 1:1.2.8-9ubuntu12.2
404 Not Found [IP: 43.255.166.254 80]
E: Failed to fetch in.archive.ubuntu.com/.../nfs-common_1.2.8-9ubuntu12.2_amd64.deb 404 Not Found [IP: 43.255.166.254 80]
E: Failed to fetch in.archive.ubuntu.com/.../nfs-kernel-server_1.2.8-9ubuntu12.2_amd64.deb 404 Not Found [IP: 43.255.166.254 80]