Hi
MCSDK: 3.1.4.7
CCS: 7
OS: win7
I could drive SRIO and NDK on C6678 before, SRIO and NDK worked simultaneously on my C6678 project correctly.
I want to drive SRIO and NDK on 66AK2H12 too, I implement SRIO and NDK driver the same as C6678 but I have an old problem, SRIO and NDK don't work simultaneously.
I followed all the tips that I used for driving SRIO and NDK on C6678 for 66AK2H12.
The only difference is core received queue numbers, I set the event ID of SRIO 49, according to datasheet as below:
So I set core received queue numbers as below:
I should mention that SRIO and NDK work well seperatly.
Please, guide me, I am under pressure for the project.
Best Regards