Hi,
My visionSDK version: 3.05.
Here is my link: qt->weston(rgb)->dssm2m(yuv422)->display
I capture picture from weston(which I read from drm device) like this:
But after DSSM2M to display link the picture like this:
Here is my DSSM2M configure:
/* DSS M2M WB link */ pPrm->enableOut = TRUE; pPrm->wbInNode = DSSM2MWBLINK_DISPC_WB_IN_NODE_LCD2; pPrm->numInPipeLines = 1U; pPrm->inPipelines[0U] = DSSM2MWBLINK_DISPC_PIPE_VID2; /* input pipeline parameters */ pPrm->inTarWidth[0U] = displayWidth; pPrm->inTarHeight[0U] = displayHeight; pPrm->inPosX[0U] = 0U; pPrm->inPosY[0U] = 0U; /* The overlay width and height are used only if 'wbInNode' is overlay node */ pPrm->ovlyWidth = displayWidth; pPrm->ovlyHeight = displayHeight; /* Output parameters */ /* Input format is ARGB32 and output format is YUV420SP_UV */ pPrm->outDataFmt = SYSTEM_DF_YUV422I_UYVY; pPrm->outWidth = displayWidth;
So is there any problem that DSSM2M will lost presion when convert RGB to YUV?
Thanks!