Hi,
I have a custom board, using Yocto for BSP customizing. For IPC in A72 linux as mentioned PSK docs there should a /dev/ entry.
I dont see any /dev entry. Is there any configuration required or I need enable any driver for the rpmsg /dev entry.
My end goal is to use user space rpmsg_char_helper library for IPC between A72(linux) <--> r5f cores (TI rtos).
Below is output log the application
root@gcp-a72:~# ./ipc_echo_test
rproc_device_find_for_name :r5f-main-0-core-0
rproc_device_find_chrdev_by_remote_port: could not find a matching rpmsg_chrdev node
Error: could not find char device by remote port: 13
Thanks