Not able to connect with USB XDC 200:IcePick_D: Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the debug probe.
Board was unpacked and verified functions.
Connector was connected to a) XDS200 and b)USB TO SOC UART0
Connector for supply connected
Programming through USB XDS 200 on board was working without troubles - programmed only demo in SDK
After weekend we were not able to connect with USB XDC 200:IcePick_D: Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the debug probe. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.1.0.00001)
All the other work places with this board worked without trouble.
New setting Target configuration
tested on the second work place > always using CCS10
Proccesor 66AKG is working, not function is only XDC 200 on board connection
Result still same. Cannot connect with debug probe
In the guide, there is for TI RTOS 06.03.00.106 at the end of chapter 10.3.4:
software-dl.ti.com/.../index_how_to_guides.html
described situation of HW destruction of emulator and it is reccomend to update FW and also update of HW. It is strange we did not find this information for evaluation kit, but only found it for TI RTOS. For review, we have modules revision A (it is already D revision)
We did not perform and HW modification. We still perform action as always. And all other evaluation kits are working without any trouble.
**The RevB and RevC boards are using an earlier version of the XDS200 firmware. We have observed the following issues when hooking up the internal XDS200 USB debug probe to a host machine.
XDS200 Emulator USB cable need to be re-plugged every time board is power cycled/reset to avoid leakage on power supply VCC1V8_XDS which can damage the regulator or other ICs.