Hi,
My customer has the following questions about CPSW.
Q1: Can the Buffer Pointer of the CPDMA receive descriptor in CPSW be assigned to MPU_RAM(0x402F_0000 - 0x402F_FFFF)?
Q2: The Broadcast Storm seems to occur when PORT1 and PORT2 are connected to the same hub.
However, even if I connect PORT1 and PORT2 to different hubs and send packets to one of them, it doesn't seem to be forwarding.
Does it reply to the received Packet with the received Port? But I don't think it's even sending it back with its own Port as it heals when I unplug one cable.
Do you have any idea if such a condition is occurring inside CPSW?
Is there a way to prevent Broadcast Storm when PORT1 and PORT2 are connected to the same hub?
Q3: Even if P2_FLOW_EN and P1_FLOW_EN of CPSW_SS_FLOW_CTRL are off, the received data of PORT1 and PORT2 can be transferred by CPDMA.
Isn't this CPSW_SS_FLOW_CTRL a function to stop the transfer of data from PORT1 and PORT22 to PORT0?
Best Regards,
H.U