Hi Team,
I am trying to create the pdk examples following the description in the link : software-dl.ti.com/.../index_overview.html
I call "C:\ti\pdk_am437x_1_0_17\packages>pdkProjectCreate.bat AM437x" on the command prompt and I get multiple errors as seen below ( same error repeats itself for all projects)
any idea what is missing ?
C:\ti\pdk_am437x_1_0_17\packages>pdkProjectCreate.bat AM437x
=========================================================================
Configuration:
SOC : AM437x
BOARD : all
ENDIAN : little
MODULE : all
PROJECT_TYPE : all
PROCESSOR : arm
PDK_SHORT_NAME : C:\ti\pdk_am437x_1_0_17\packages\
=========================================================================
Checking Configuration...
Complete
=========================================================================
PDK_PARTNO : AM437
PDK_ECLIPSE_ID : com.ti.pdk.am437x
RTSC_PLATFORM_NAME : ti.platforms.evmAM437X
RTSC_TARGET : gnu.targets.arm.A9F
CCS_DEVICE : "Cortex A.AM4379.IDK_AM437X"
*****************************************************************************
Detecting all projects in PDK and importing them in the workspace C:\ti\pdk_am437x_1_0_17\packages\\MyExampleProjects
Detected Test Project: EMAC_BasicExample_evmAM437x_armBiosExampleProject
The system cannot find the path specified.
Copying macro.ini
The system cannot find the path specified.
0 file(s) copied.
Detected Test Project: EMAC_BasicExample_idkAM437x_armBiosExampleProject
The system cannot find the path specified.
Copying macro.ini
The system cannot find the path specified.