Hi ,
Do we need to do changes in u-boot-k3-r5 for booting from OPSI ? Is OPSI boot will work with SD card (MMC) boot image built ?
If need to changes the boot image for OPSI then what are the config parameter need to add. And also OPSI can work with file partition table same as SD card ?
Currently our build is with TI sdk 6.02.00 .
Thanks and Best Regards,
Shrinath