Other Parts Discussed in Thread: AM3358, AM5729, AM5728
Tool/software: Code Composer Studio
Hi,
The new SDK documentation is more helpful and streamlined from the Wiki, but its generic, or at least in the PRU section as largely relates to the BeagleBone Black.
I'd posted previously about where to find the specific SDK for each chip family, there were family links on each CPU page (such as having AM335x, or AM572x in the path), but now it seams that they all link to the standard SDK page which in the PRU section is AM335x based etc.
My issue is that I'm trying to follow the Hands on labs and create a PRU project for this board.
There is only the list of processors, TI dev board, and then Beaglebone/Beaglebone Black, no BeagleBone AI.
For the moment, do I select IDK_AM572X? I believe its an industrial communication dev board, so will have a bunch of Ethernets etc on it, and some other ports like SATA, which is very different from the AI, but same processor.
If I have to still select the BeagleBone Black as the board in CCS for the project, that may be ok for PRU binaries, but then I won't have an option to make M4 or C6600 ones I assume.
The main CPU difference between the Black (AM3358) and AI (AM5729) is: 2 extra PRU, 2 additional Cortex M4 (instead of single M3), dual Cortex A15 instead of single A8. Then more graphics and video encoding etc.
Thanks,
Fisher