Hi all,
When am57xx boot from nand the sysboot PINs conflict with GPMC_ADx, how to workaround this? thanks!
BR,
Denny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
When am57xx boot from nand the sysboot PINs conflict with GPMC_ADx, how to workaround this? thanks!
BR,
Denny
Denny,
Can you please confirm the hardware and software combination in which this issue is being seen?
Regards
Karthik
Thanks for your reply!
The schematic diagram is attached.
I want to boot from NAND flash device, but the ad pin of NAND flash (GPMC interface) is multiplexed with sysboot pin. Sysboot pin is pulled down to 1V(as shown in the figure) when AM5728 during startup, and sysboot cannot identify which device to boot from. Is it necessary to add isolation chip between am5278 and NAND?Or the resistance between them (75 Ω) is too large?Thank you!
The ADx pins are floating during reset - neither the processor or flash memory device are driving. Therefore using pullup or pulldown resistors - you can set the SYSMODE value. From you schematic snip-it - it appears you have both pull-up and pull-down resistor(s) installed. This is set the voltage in the middle - 1.5V. You should install either pull-up or pull-down resistor based on what SYSMODE value you wish - but never install both pull-up and pull-down on same net.