Hi,
SDK:ti-processor-sdk-rtos-c667x-evm-06.03.00.106
Is there only one example (ex11_ping) of IPC?
ti-processor-sdk-rtos-c667x\ipc_3_50_04_08\examples\C6678_bios_elf\ex11_ping
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
SDK:ti-processor-sdk-rtos-c667x-evm-06.03.00.106
Is there only one example (ex11_ping) of IPC?
ti-processor-sdk-rtos-c667x\ipc_3_50_04_08\examples\C6678_bios_elf\ex11_ping
Hi,
Customer want to use Notify module.
There are some code in the below link, is there a complete project (or at least .c file and .cfg file) based on the latest SDK?
Hi, Nancy,
Your question is asked in the other thread, e2e.ti.com/.../942954
I'll have the IPC expert to answer it in that thread and close this one. Thanks!
Rex