Part Number: EVMK2G
Tool/software: Code Composer Studio
Hi,
I am facing some issues while creating a project folder. I am using EVMK2G board. I have an example project created using the command "pdkProjectCreate.bat K2G all little uart all dsp". This project uses tirtos and works.
For practice purposes I wanted to test the UART-EDMa interface using baremetal (without using TIRTOS/Linux).
I have created a project with BARE_METAL settings and copied all the necessary source code and header files. I have got few linker errors which I could not resolve.
1. _CSL_intcCpuIntrTable ./src/ti/pdk_k2g_1_0_16/packages/ti/csl/src/intc/_csl_intcIsrDispatch.obj
2. _c_int00 ./src/ti/pdk_k2g_1_0_16/packages/ti/csl/src/intc/_csl_intcIsrDispatch.obj
CSL_intcCpuIntrTable is defined in _csl_intcResource.c and have included that source file in my project. Still the linker error exists
c_int00 is defined in boot.c and have included that also. Still the linker error exists
I have below questions
1. Can the EDMA-UART interface work using BARE_METAL and without use of TIRTOS?
2. In the project file I have excluded some source files but not able to include them again. what is the way to do it?