Hi,
According to the "Figure 4. Power Sequencing of TPS65911A User's Guide for 66AK2G12 Processor"
the time slot from launch of 3.3V to launch of 1.8V, 1.35 V and 1.0V is 2~5ms.
If this time slot is 12~28ms, is there any problem?
We are considering implementation with discrete power supplies and TPS3808G01 on behalf of PMIC.
The delay time of TPS3808G01 is 12ms~28ms.
Thanks.