This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TMS320C6678: How do I enable jumbo packet support on C6678?

Guru 80195 points

Replies: 1

Views: 35

Part Number: TMS320C6678

The default NDK/NIMU example only supports regular Ethernet packet (1514 bytes). The article describes how to enable NDK/NIMU driver and test for the jumbo packet support on TI C6678 device.

When enabling/testing for other TI Keystone I/II devices:

  • The NDK package is device independent, the same changes can be kept.
  • However, NIMU driver is device dependent, user expects to find and implement the change in the respective NIMU driver.
  • Test methodology should apply to all devices.   

Regards, Eric  

Enabling Jumbo Packet Support for C6678.pdf

  • Guru 80195 points

    Thanks for the information!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.