Other Parts Discussed in Thread: TMDSEVM437X
Hi experts,
My customer is connected to the AM437xEVM from his PC via a full-speed USB hub. After sending descriptors from the EVM to the PC in this situation, the USB goes into a suspended state and cannot be connected.. Can AM437xEVM communicate via a USB hub of Full-Speed?
Incidentally, he also tried another USB hub, but it failed to connect with the same problem.
My customer's SW : USB_DevBulk_evmAM437x_armExampleProject or USB_DevMsc_evmAM437x_armExampleProject (pdk_am335x_1_0_16)
My customer's HW : TMDSEVM437X
Best regards,
Sasaki