Hi,
When I run MCSPI on EDMA mode in IPU1 only, it went fine.
But when I startup visionSDK on IPU2, DSP, EVE, MCSPI EDMA seems overload. Because it will get Rx overflow interrupt occasionly and Tx complete event sometimes be triggered too late.
MCSPI Tx and Rx event queue number is 0.
When I print "Statistics Collector":
[HOST] [IPU2 ] 177.074940 s: STATISTIC Avg Data Peak Data ^M [HOST] [IPU2 ] 177.075032 s: COLLECTOR MB/s MB/s ^M [HOST] [IPU2 ] 177.075123 s: -------------------------------------------------- ^M [HOST] [IPU2 ] 177.078021 s: SCI_EDMA_TC0_RD | 0.412712 0.749414^M [HOST] [IPU2 ] 177.078143 s: SCI_EDMA_TC0_WR | 0.412273 0.761143^M [HOST] [IPU2 ] 177.078234 s: SCI_EDMA_TC1_RD | 102.411935 798.352373^M [HOST] [IPU2 ] 177.078387 s: SCI_EDMA_TC1_WR | 102.426202 798.532582^M
TPTC0 is MCSPI used and TPTC1 is used by camera, seems they have no concurrent, but could it be possible it overrun on TPCC? Or would you please give me some hint of this bug?
Thanks a lot!
BR/Tim