This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

PROCESSOR-SDK-AM437X: Evaluation kit for AM437x:TI-RTOS:Ethernet/IP

Expert 1320 points

Replies: 2

Views: 41

Part Number: PROCESSOR-SDK-AM437X

HI,

there are three eval kit provided by TI am437x.

1) AM437x high security evaluation module

TMDSEVM437X
2) AM437x/AMIC120 Industrial Development Kit (IDK)
TMDSIDK437X
3)AM437x Starter Kit
TMDXSK437X
4) TPS65218 Evaluation Module
TPS65218EVM-100
Which one should i purchase?
my requirement is as mentioned below.
I want to use AM4376.
I want to use TI-RTOS and not linux.
1) To develop Ethernet/IP adapter with DLR redundancy.
2) Also want to use secure Boot feature and other security related features 
3) Also want to run tfftp server, ftp server, sntp client, https server, snmp v3 agent and other network services along with EIP adapter with DLR.
Regards,
Vrund

  • Hello Vrund,

     

    The different EVMs are available for our customers to evaluate different use cases.

    • If you need to evaluate secure boot, you would need to use the High Security EVM that you list down at the top. 
    • TMDSEVM437X https://www.ti.com/tool/TMDSEVM437X
    • But, before purchasing the EVM, you would need a special security NDA established with TI. You can submit the request and you will find this at the above link.

     

    • If you don't need to security right away, easy way is to get the Starter Kit (TMDXSK437X) which costs just $299.

     

    • TMDSIDK437X is designed to let our customer evaluate specific functions in motor control, factory automation.

     

    • TPS EVM you reference above is only for the TPS device..
    • The AM4x EVMs will have this device already but the TPS EVM will not have AM4x.

     

    Hope this clarifies the different options.

    Please also note that for a limited time, we do have a discount coupon for the AM4x above. You will see this code right on the tool page.

    Thanks

    Srik Gurrapu

  • In reply to Srik%20Gurrapu:

    Hello,

    is Ethernet/IP adapter  functionality for AM4376 can be evaluated by below mentioned 

    eval board.

     AM437x high security evaluation module

    If no then in that case i have to purchase two eval boards right?
    which other board should i go to evaluate Ethenet/IP adapter functionality for am4376?
    Regards,
    Vrund

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.