Hello,
I recently upgraded to SDK version 06.03.00.106, and have noticed that something related to WiFi is taking a very long time to load during the boot. The kernel goes through it's whole boot process and gets to the login screen, and then approximately two minutes later I get the following printout:
[ 127.865844] NET: Registered protocol family 15
[ 128.371934] Initializing XFRM netlink socket
Before this prints out, WiFi does not work. I also have a program setup to run after boot, and the program does not run until after these messages are printed out. But this only happens if I run everything off of the SD card. If I use the NFS for the filesystem, I don't have this problem. Any ideas about what is going on?