Hi Team,
I am testing boot from uart and than load application from uart and execute it
I would like to use the led blink sk demo (TI RTOS) for this test.
I am doing so on the AM437x SK, which was modified to boot from UART.
After boot , when looking at the terminal I get 'C' printed continuously which, as I understand indicates that the SK is in UART boot mode.
How do I go about actually downloading the application and executing at this stage ?
is there anything I should do for the application output file before I download it with the uart ?