When I was debugging the TDA4+AR0233 camera, the image display was not normal. The relevant information is as follows
Board : J721E-EVM
SDK Version: rtos-07_01_00_11
Demo App : run_app_single_cam.sh(vx_app_single_cam.out)
Camera: AR0233+DS90UB953
Camera Model : Sensing SG2-AR0233C-FPDLink
Camera Parameter: 1920x1080,30 fps,Bayer RAW12
Connection: TDA4->DS90UB960->Camera
I have tried to modify part of the configuration in ar0233 drievers(iss_sensor_ar0233.h/iss_sensor_ar0233.c/ar0233_serdes_config.h), and the result is the same. Can you identify the possible problems, such as the camera configuration error or UB960 configuration error or CSI transmission error?img_rawdata.zip2158.log.zip