I have u-boot env stored in MMC and default values in code get stored in MMC and works fine.
I want to add few objects/modify from linux. I tried to use fw_printenv/fw_saveenv , which didnt work.
I think the best option would be to use uEnv.txt.
So I copied my default env to uEnv.txt and stored in /dev/mmcblk0p2, which is n ext4 file system and gave the name as entry in u-boot configuration
The uboot code tries to read the file from ext4 file system , it reads the file but says CRC32 error and then load defaults from the MMC. I have been trying to solve this for few days
Any help appeciated