This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U: The division of the domain that is independent as a die and also supplies power individually.

Part Number: DRA821U

Hi

Please tell me the division of the domain that is independent as a die and also supplies power individually.

Are they divided into only 2 parts, MAIN and MCU which includes WKUP?

Thanks and Best regards,

HaTa.

 

  • Hi HaTa,

    HaTa said:
    Are they divided into only 2 parts, MAIN and MCU which includes WKUP?

    The device has three domains: (please see Figure 1-1. Device Top-level Block Diagram in the TRM)

    1. WKUP

    2. MCU

    3. MAIN

    You can read about the functionality/significance of each in the subsequent sections.

    HaTa said:
    Please tell me the division of the domain that is independent as a die and also supplies power individually.

    If you are looking from operating independent of each other then the chip supports functionality of the MCU working on its own independent of the MAIN domain. 

    You can read about in 5.2.3.Device Power States in the TRM.

    Regards,

    Karan

  • Hi Karan

    Thanks!