Other Parts Discussed in Thread: DRA821
Hi
Please provide the list about ambient temperature for each DRA821x?
I can find only Junction temperature in DM.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I do not understand the question. Can you elaborate?
What is the operating temperature range of the DRA 821?
Only the junction temperature specifications are listed on the data sheet.
I would like to know the ambient temperature specifications ,which the DRA821 can be opereated normally.
Hi Kevin
I appreciate if you give us your comment for
>What is the operating temperature range of the DRA 821?
>Only the junction temperature specifications are listed on the data sheet.
>I would like to know the ambient temperature specifications ,which the DRA821 can be opereated normally.
Thanks and Best regards,
HaTa.
The junction temperature is the critical parameter.
Since the storage temperature shows a range of -55C to 150C, it is necessary that the device is NOT harmed at those temperatures. However, the operating range is -40C to 125C (for automotive class devices). This means that the die must operate within this range. If the temperature were colder than -40C and the system was sometimes turned OFF, there would be times operating outside of the limits. Similarly, the junction is almost always hotter than the ambient. In a high power operation, the system must transfer heat from the device to the ambient in order to maintain its 125C junction limit. It is therefore typical that the ambient is not nearly as hot as 125C.
There is no ambient specification beyond the storage temperature cited earlier and the limits imposed by the junction temperature.
Kevin