Other Parts Discussed in Thread: OMAPL138
Hi,
I am trying to enable httpd package into my yocto build, steps I followed is as below
1. Added below layer in bblayer.conf file
sources/meta-openembedded/meta-webserver
2. Added below line in local.conf file
IMAGE_INSTALL_append = "apache2"
The yocto build using bitbake core-image-minimal gives below error
WARNING: core-image-minimal-1.0-r0 do_rootfs: busybox.postinst returned 1, marking as unpacked only, configuration required on target.
ERROR: core-image-minimal-1.0-r0 do_rootfs: Postinstall scriptlets of ['busybox'] have failed. If the intention is to defer them to first boot,
then please place them into pkg_postinst_ontarget_${PN} ().
Deferring to first boot via 'exit 1' is no longer supported.
Details of the failure are in /home/h440246/Projects/rfid/BSP/tisdk/build/arago-tmp-glibc/work/omapl138_lcdk-oe-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.
ERROR: core-image-minimal-1.0-r0 do_rootfs: Function failed: do_rootfs
ERROR: Logfile of failure stored in: /home/h440246/Projects/rfid/BSP/tisdk/build/arago-tmp-glibc/work/omapl138_lcdk-oe-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.2937
ERROR: Task (/home/h440246/Projects/rfid/BSP/tisdk/sources/oe-core/meta/recipes-core/images/core-image-minimal.bb:do_rootfs) failed with exit code '1'
Please provide the solution for the same
With Best Regards,
Sharmila D