This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6528: USB to connect to the hub

Part Number: AM6528

Hi

Like to understand how to connect the USB port to a hub chip? Below is what i think should be done please let me know if this is correct or not?

How should one properly deal with the secondary USB pins when hard wiring them to a USB hub chip?

 

For the USBx_ID, I am going to tie this to a ground (via resistor) to default the AM65’s port to be the USB master.

 

USBx_VBUS:  I was going to hardware this thru a resistive network to always be at 1V.  This circuit will consist of a 3.3V supply (always on) with two resistors to set the voltage on the pin.  Does this pin need to toggle due to changes with USBx_DRVVBUS?     

 

USBx_DRVVBUS:  This signal is going to be left unconnected.

Thanks