How to capture screen using drm api? how to get the frame buffer and pass it to GStreamer api.
I`m using IOCTl
int main()
{
//------------------------------------------------------------------------------
//Opening the DRI device
//------------------------------------------------------------------------------
int dri_fd = open("/dev/dri/card0",O_RDWR | O_CLOEXEC);
//------------------------------------------------------------------------------
//Kernel Mode Setting (KMS)
//------------------------------------------------------------------------------
uint64_t res_fb_buf[10]={0},
res_crtc_buf[10]={0},
res_conn_buf[10]={0},
res_enc_buf[10]={0};
struct drm_mode_card_res res={0};
//Become the "master" of the DRI device
ioctl(dri_fd, DRM_IOCTL_SET_MASTER, 0);
//Get resource counts
ioctl(dri_fd, DRM_IOCTL_MODE_GETRESOURCES, &res);
res.fb_id_ptr=(uint64_t)res_fb_buf;
res.crtc_id_ptr=(uint64_t)res_crtc_buf;
res.connector_id_ptr=(uint64_t)res_conn_buf;
res.encoder_id_ptr=(uint64_t)res_enc_buf;
//Get resource IDs
ioctl(dri_fd, DRM_IOCTL_MODE_GETRESOURCES, &res);
printf("fb: %d, crtc: %d, conn: %d, enc: %d\n",res.count_fbs,res.count_crtcs,res.count_connectors,res.count_encoders);
void *fb_base[10];
long fb_w[10];
long fb_h[10];
//Loop though all available connectors
int i;
for (i=0;i<res.count_connectors;i++)
{
struct drm_mode_modeinfo conn_mode_buf[20]={0};
uint64_t conn_prop_buf[20]={0},
conn_propval_buf[20]={0},
conn_enc_buf[20]={0};
struct drm_mode_get_connector conn={0};
conn.connector_id=res_conn_buf[i];
ioctl(dri_fd, DRM_IOCTL_MODE_GETCONNECTOR, &conn); //get connector resource counts
conn.modes_ptr=(uint64_t)conn_mode_buf;
conn.props_ptr=(uint64_t)conn_prop_buf;
conn.prop_values_ptr=(uint64_t)conn_propval_buf;
conn.encoders_ptr=(uint64_t)conn_enc_buf;
ioctl(dri_fd, DRM_IOCTL_MODE_GETCONNECTOR, &conn); //get connector resources
//Check if the connector is OK to use (connected to something)
if (conn.count_encoders<1 || conn.count_modes<1 || !conn.encoder_id || !conn.connection)
{
printf("Not connected\n");
continue;
}
//Kernel Mode Setting (KMS)
//------------------------------------------------------------------------------
printf("%d : mode: %d, prop: %d, enc: %d\n",conn.connection,conn.count_modes,conn.count_props,conn.count_encoders);
printf("modes: %dx%d FB: %d\n",conn_mode_buf[0].hdisplay,conn_mode_buf[0].vdisplay,fb_base[i]);
struct drm_mode_get_encoder enc={0};
enc.encoder_id=conn.encoder_id;
ioctl(dri_fd, DRM_IOCTL_MODE_GETENCODER, &enc); //get encoder
struct drm_mode_crtc crtc={0};
crtc.crtc_id=enc.crtc_id;
ioctl(dri_fd, DRM_IOCTL_MODE_GETCRTC, &crtc);
printf("Next : %s : %d\n",crtc.mode.name, crtc.fb_id);
}
fflush(stdout);
//Stop being the "master" of the DRI device
ioctl(dri_fd, DRM_IOCTL_DROP_MASTER, 0);