Part Number: TMDX654GPEVM
Hello everyone,
I want to update the uboot old version to sdk7:
what i do:
#cd /home/jmiao1/sdk/am65xx-07/bin/
#sudo ./mksdboot.sh --device /dev/sdd --sdk /home/jmiao1/sdk/am65xx-07/
but when i used this sd to boot the am65x board, there is not anything print. Why ?
old version
U-Boot SPL 2018.01-gcdb1cc0a9e (Oct 06 2018 - 03:46:53) SYSFW ABI: 2.4 (firmware rev 0x0012 '18.8.2-v2018.08b (Curious Crow)') Trying to boot from MMC2 Starting ATF on ARM64 core... NOTICE: BL31: v1.5(release):ti2018.03-rc1 NOTICE: BL31: Built : 02:55:53, Oct 6 2018 I/TC: I/TC: OP-TEE version: 3.2.0-81-g48952f9-dev #1 Sat Oct 6 03:34:58 UTC 2018 aarch64 I/TC: Initialized U-Boot SPL 2018.01-gcdb1cc0a9e (Oct 06 2018 - 03:44:38) Trying to boot from MMC2 U-Boot 2018.01-gcdb1cc0a9e (Oct 06 2018 - 03:44:38 +0000) Model: Texas Instruments AM654 Base Board I2C: Error, wrong i2c adapter 0 max 0 possible ready DRAM: 4 GiB MMC: sdhci@0: 0, sdhci@0: 1 Error, wrong i2c adapter 0 max 0 possible In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: eth0: cpsw_nuss@046000000 Hit any key to stop autoboot: 0 Booting from network ... ... link up on port 1, speed 100, full duplex Using cpsw_nuss@046000000 device TFTP from server 128.224.162.214; our IP address is 128.224.162.200 Filename 'Image'. Load address: 0x80080000 Loading: ################################################################# ################################################################# ###########################################################