Other Parts Discussed in Thread: TMDX654IDKEVM, CLOCKTREETOOL
In the R core on TMDX654IDKEVM,
We are verifying the access time to MCU_MSRAM and DDR.
question 1
Please tell me about the theoretical value (MHz) at the time of Read / Write from R core to MCU_MSRAM and DDR when 400MHz is supplied to R core.
Below are additional questions.
Additional question 1
The access route from the R core to the MCU_MSRAM is
"R core → MCU_CBASS0 → MCU_MSRAM"
Are you sure?
Also, the access route to DDR is
"R core → MCU_CBASS0 → CBASS0 → NAVSS → MSMC → DDRSS"
Are you sure?
Additional question 2
I have confirmed it on ClockTreeTool (AM65xSR2.0).
0x00000001 in CTRLMMR_WKUP_MAIN_SYSCLK_CTRL
0x00008000 in WKUP_PLLCTRL0_PLLDIV1
Set, and
When 400MHz is supplied to MCU_R5_CORE0,
200MHz and 100MHz are supplied to MCU_MSRAM0.
Is it okay to understand that it operates at 200MHz when reading and writing data and at 100MHz when changing settings?
MCU_CBASS0 is supplied with 200MHz, 100MHz and 50MHz,
Does 200MHz and 100MHz apply to access to MCU_MSRAM0?
In addition to the above, is it okay to recognize that it operates at 200MHz when reading and writing from the R core to the MCU_MSRAM?
Best regards