Hello Guys,
Good day.
The contents of the TMS320C6713 DSP Starter Kit (DSK) from TI site were not specified. Could you confirm that it contains all that were specified on the link below specially the 2M x 32 SDRAM ?
Thanks in advance!
Art
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Guys,
Good day.
The contents of the TMS320C6713 DSP Starter Kit (DSK) from TI site were not specified. Could you confirm that it contains all that were specified on the link below specially the 2M x 32 SDRAM ?
Thanks in advance!
Art
Please refer to the contents of the Kit from TI as below:
The link you provided is not a TI link.
Hello Art,
I can't comment on non-TI link (3p link).
From TI's link, I see below:
The DSK features the TMS320C6713 DSP, a 225 MHz device delivering up to 1800 million instructions per second (MIPs) and 1350 MFLOPS. This DSP generation is designed for applications that require high precision accuracy. The C6713 is based on the TMS320C6000 DSP platform designed to needs of high-performing high-precision applications such as pro-audio, medical and diagnostic. Other hardware features of the TMS320C6713 DSK board include:
Thanks,
Aravind
Hello Art,
I am closing the thread as there is nothing else to discuss on this thread.
Thanks