Hi All,
We are using PROCESSOR_SDK_VISION_03_07_00_00 in our custom board. Our HW is meant for 2 stage QSPI boot. In this process the device is supposed to take MLO and uboot from QSPI device and
it should take the file system from eMMC.
After booting from SD card I have flashed uboot and MLO in the QSPI. Also I have flashed eMMC with the follwing command:
fdisk /dev/mmcblk1
o // for starting a new partition
p // to list the current partitions
n // to create new partitions
Enter p for primary
Enter
+3000M // to get 3 GB eMMC block
w // To write the changes to eMMC. After this the fdisk prompt is exited
umount /dev/mmcblk1p1
mkfs.ext4 /dev/mmcblk1p1
reboot
Now place and extract the filesystem placed in SD card /var/ti_sdk.tar.xz to /run/media/mmcblk1p1
cp /var/ti_sdk.tar.xz /run/media/mmcblk1p1
tar xvf ti_sdk.tar.xz
But with this my board gets stuck in uboot when I remove the SD card.
Can anyone please tell me which step I have missed ?
Thanks,
Deepika