Hi, TI experts.
We are working on several cameras connect to CSIRX via max9286/max9296 deserializes. There are several combinations that we tried.
(we are using PSDK7.01)
case 1: One camera + max9286 with single_cam_example (works, image captured correctly)
case 2: 4 camera + max9286 with multi_cam_example (does not work)
case 3: 1 camera + max9296 with single_cam_example (does not work)
As we use YUYV camera, we skipped all VISS, LDC nodes and configure a CSIRX -> DP display graph.
In all those cases, we could measure correct MIPI signals on the CSIRX pins, for example, the second case:
There is no image when we run the camera capture examples for case 2, case 3. (And no error either.)
We measured the MIPI clk and believe set the correct data rate. still no luck.
Please, how can we figure out the cause of the problem? which registers do we need to check? Is there a procedure we can follow to debug?