Hi,experts:
1. When use FFmpeg to decode H264 bitstream which encoded by TDA4, then I get every frame and store in .jpeg files.
Below is my commands:
`ffmpeg -i encode_output.h264 image-%05d.jpeg`
After that I check the .jpeg files, there are some duplicate frames. For example, frame 99 and frame 100 are the same, frame 101 are changed.
There are no duplicate frames when I save the MSC Mosaic output .yuv files, so I think the duplicate frames was generated when TDA4 encodeing.
2. How can I solve this problem?
3. Environment:
a. RTOS SDK: 07_02_00_06
b. vision_apps/apps/basic_demos/app_encode/
c. encode parameter is default
Thanks.