I have two versions of NDK installed on a device and are evaluating TCP / IP.
・ Ndk_2_25_01_11
・ Ndk_3_40_01_01
Multiple devices are connected to the switching HUB.
In the case of normal communication, there is a response within 1ms to the transmission from the host,
When ARP is sent from one device, the response time of another unrelated device is delayed (about 200ms).
It occurs in ndk_2_25_01_11, but it does not occur in ndk_3_40_01_01. Did you fix it in the process of version upgrade?
I am being asked to explain why.