Hello,
Can we use 500Ohm 5% for USB1_RCALIB and USB0_RCALIB resistor values, We are not using the same section (USB Interface USB0 and USB1) in our application.
Thanks
Arun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can we use 500Ohm 5% for USB1_RCALIB and USB0_RCALIB resistor values, We are not using the same section (USB Interface USB0 and USB1) in our application.
Thanks
Arun
Arun,
We can't guarantee USB performance with a 5% resistor. I'm not sure I understand this part of your question:
"We are not using the same section (USB Interface USB0 and USB1) in our application." What do you mean by section? And what are you comparing your application to?
Best Regards,
Zack
Hello Zack,
The entire USB section is not connected and we are not using the interface. As I gone through the datasheet it is mentioned to keep a 500 ohms calibration resistance. Is it mandatory to pull down even if we are not using the USB peripheral.
Regards
Arun